AXIS#.UNIT.VLINEAR
Description
AXIS#.UNIT.VLINEAR sets the units type for the velocity parameters when the motor type (AXIS#.MOTOR.TYPE ) is linear.
Type |
Description |
---|---|
0 |
counts/s |
1 |
mm/s |
2 |
µm/s |
3 |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
0 to 3 |
Default Value |
1 |
Data Type |
Integer |
See Also |
AXIS#.VL.FB , AXIS#.VL.CMDU , AXIS#.VL.CMD, AXIS#.MOTOR.TYPE |
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
AXIS1.UNIT.VLINEAR |
5010h |
08h |
Unsigned8 |
- |
- |
Read/Write |
No |
AXIS2.UNIT.VLINEAR |
5110h |
08h |
Unsigned8 |
- |
- |
Read/Write |
No |
Name |
ID |
Hex |
Data Type |
Access |
Units |
---|---|---|---|---|---|
AXIS1.UNIT.VLINEAR |
6606 |
19CE |
Unsigned8 |
Read/Write |
- |
AXIS2.UNIT.VLINEAR |
72142 |
119C |
Unsigned8 |
Read/Write |
- |
Parameter |
PNU |
Data Type |
Access |
Units |
---|---|---|---|---|
AXIS#.UNIT.VLINEAR |
6606 |
Unsigned8 |
Read/Write |
- |